7/20/2014 9:59 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
But it is a question or you really this happens? |
7/24/2014 7:02 PM | |
Posts: 5225 Rating: (1185) |
It is a bit more difficult than simply "either or". It goes to the voltage and frequency that the motor coils receive. The motor is rated for 230V Y / 400V Δ. With the motor is connected to Δ (delta), the motor prefers that the line-to-line voltage not exceed 230V. Please check these notes.. [LINK1] [LINK2] with [LINK3] Greetings. w |
Follow us on