8/20/2014 4:16 PM | |
Posts: 5225 Rating: (1192) |
See if the image attached help you. |
This contribution was helpful to1 thankful Users |
8/20/2014 9:47 PM | |
Posts: 5225 Rating: (1192) |
Hi there, Please find attached another design idea that uses bits to set visibility. In the ZIP attachment contains 2 JPEGs, a simulation parameter set and a sample program. The first JPEG shows how to activate the simulation. Trigger BIT1 and BIT2 on and off to see the result. The trick in this example is that the a part of the image is now in two segments and the layering position is important. See if this can work for you.. I'd like for you to give some feedback. Greetings. w AttachmentDesign Idea_Control visibility of overlayed pictures.zip (230 Downloads) |
8/20/2014 10:43 PM | |
Posts: 5225 Rating: (1192) |
This example completes the set. It shows how objects can be moved. This uses x2 INT values.. in this case each from 0..9 in value. The images are image segments that are grouped together. The groups are then moved from position using the "animation" function (right click on an object/group for quick access). I recommend you look at the previous example first and then this one. This example does not contain instructions on how to trigger the simulation. A JPEG displaying what to expect is included. The simulation parameters are also included with project sample. I hope you find this helpful. w AttachmentDesign Idea_Control position of grouped segmented pictures.zip (164 Downloads) |
Follow us on