Industry Online Support
Technical Forum
6/5/2013 11:17 AM | |
Posts: 18 Rating: (0) |
Hello guys! I have to make a function block for controling a danfoss vlt 5000 drive with ppo 3 type. I attach a file with an exemple.I didn't undersand exacly what's happen.Can somebody explain step by step in my example?Just delete my comments and write for every step(line) from the program. Many thanks. AttachmentDanfoss control drive.zip (500 Downloads) |
Last edited by: O_Moderator at: 6/7/2013 8:33 AMnew subject after splitting from /tf/WW/en/Posts/56792#top |
|
10/16/2013 3:21 PM | |
Posts: 29 Rating: (2) |
I'm not sure about VLT 5000 series. May be it's obsolete. The only current industrial drives from Danfoss is listed at the following page. http://www.ctiautomation.net/Danfoss-Drives.htm |
10/16/2013 3:56 PM | |
Joined: 4/24/2006 Last visit: 5/2/2024 Posts: 8629 Rating: (1147) |
Hello, Yes, the VLT5000 serie is obsolete See attachment for communication setup between S7 and VLT5000 through Profibus And here is a link to download functionblocks: http://www.danfoss.com/BusinessAreas/DrivesSolutions/profibus Best regards, Wizard Attachmentdoc_A_1_mc50a202.pdf (404 Downloads) |
Last edited by: Wizard at: 10/16/2013 3:58 PM |
|
1/14/2014 8:22 AM | |
Posts: 18 Rating: (0) |
I have finnaly succeeded to finish the function for control an danfoss drive with PPO 3 type telgram.Can somebody look on my file(see attachments) and see if the code and comments are good? Many thanks! AttachmentDanfoss control drive.zip (497 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on