8/19/2019 2:34 PM | |
Joined: 5/21/2018 Last visit: 7/12/2021 Posts: 49 Rating: (1) |
Hello Support team, I have created a simple function called “Simple Calculation“ with 2 inputs iInput1 and iInput2 which are integers and have set as return function as integer. I call this function in a function block and set the outputs as shown in the picture above. I have to write the code of return. But its not clear, so I am getting an error. Can some one put here the code a simple example of a function with return which is called in a function block. Looking forward to hear your response. Here with i attach you a pdf with snap shot. Thank you With regards john Attachmentfunctionwithreturn.pdf (182 Downloads) |
8/19/2019 4:28 PM | |
Joined: 5/21/2018 Last visit: 7/12/2021 Posts: 49 Rating: (1) |
Thank you for the Tip. It works. |
Follow us on