9/5/2015 5:12 AM | |
Posts: 22 Rating: (0) |
Dear All: Hello, I use one Smart S7-200 PLC to do the USS communication with one piece G120(CU240B-2, PM240-2), I use 1ph 220V to do the inverter power supply as for temporary. the PLC software is written follow the template example, and the same softeware communicate MM440 well. I connect the G120 and S7-200 smart PLC. the G120 display the BF light flash 2-3 seconds/ times . and I give the run signal the G120 display the run status, and the display setpoint frequency is correct with PLC software. but after about 30 seconds, G120 display the F1910, and I use P2118 to ignore the error, and the new error F7802 and F30027 will display. could you please help me to check? Thanks a lot. AttachmentUSS.zip (134 Downloads) |
Follow us on