9/10/2018 6:29 AM | |
Joined: 11/2/2015 Last visit: 10/16/2021 Posts: 39 Rating: (0) |
Dear all ! I also want to use Sinamics G120C without Profibus. I have a motor. I want a that motor run by 3 speeds is 15Hz, 35Hz and 50Hz. By supply +24VDC for DI1 then motor run in speed is 15Hz, similar for DI2 , DI3 I want to set parameter of it by TIA What do I need to set parameters ? Please help me ! Thank ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/10/2018 1:37:49 PMNew subject after splitting |
|
9/10/2018 2:52 PM | |
Joined: 10/11/2006 Last visit: 4/24/2024 Posts: 5823 Rating: (789)
|
Hello, you can use fixed speed setpoint as setpoint source with direct selection. |
With best regards, |
|
9/19/2018 2:40 AM | |
Joined: 11/2/2015 Last visit: 10/16/2021 Posts: 39 Rating: (0) |
Dear I will continous study about it When i have real G120C i will try And will feedback later. Thank ! |
Follow us on