4/8/2019 12:46 PM | |
Posts: 6 Rating: (0) |
Hi Everybody, Currently I've to develop a system to control an small hoist. The system is driven by a G120 with a CU250S-2 PN (5kW) controlled by an Encoder (incremental encoder). Which parameters I should consider to be sure that the hook connected at the hoist NOT fall down on someone's head when I move the hoist?How do I use the encoder to control the position on order to have a full control on the motor? Thank you in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/8/2019 2:25:50 PMNew subject after splitting |
|
Follow us on