9/30/2020 12:51 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (296) |
Hi, of course it is possible to acyclically write parameters from the PLC to the drive. For G120X this is a little tricky as you need to know the sequence of commissioning etc. Therefore there is an application available. It is a TIA AddIn which can create a PLC program to acyclically write parameters. The app is available in general - BUT: For the G120X specifically there is an extension available. See this application here: https://support.industry.siemens.com/cs/de/en/view/109777633 There is a note at the bottom that you should get in contact with your local Siemens sales partner to use this application extension for G120X. |
Best regards, |
|