3/5/2020 4:35 PM | |
Posts: 3 Rating: (0) |
For some reason my computer is not recognizing the board at all. Nothing comes up in device manager and I have installed the drivers for the Galileo Gen 2 board. Does anyone know how I can fix this? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/06/2020 09:24:05New subject after splitting |
|
3/6/2020 3:01 PM | |
Posts: 3 Rating: (0) |
Hi Fe_lipe, I am using Windows 10 Enterprise 1809. I don't see the board on the Arduino IDE. I have downloaded the galileo packages on Arduino IDE. I believe Arduino IDE is not seeing the device because my computer isn't seeing the IOT2000 on the device manager. I thought to fix this, I had to download the drivers from here: https://downloadcenter.intel.com/download/26417/Intel-Galileo-Firmware-Updater-and-Drivers?product=83137 When I downloaded IntelGalileoWindowsSerialDrivers.zip and unzipped it, the only two files in the folder were a .cat file and .inf file. I right clicked and downloaded the .inf file and it said the operation completed successfully. However, when I connect the IOT2000 to my computer using the micro USB port, the device still does not come up on device manager so it does not come up on Arduino IDE. I also downloaded IntelGalileoFirmwareUpdater-1.1.0-Windows.zip to update the driver. That folder contains the same two files as the SerialDrivers zip file and an .exe file. When I opened the .exe file, the Port drop down menu does not see the device either. |
Follow us on