11/11/2015 1:54 PM | |
Posts: 1 Rating: (0) |
Hello Guys, Is there any Gateway Converter at Lowest price. Suggest me some make. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/11/2015 2:53:13 PMNew subject after splitting |
|
11/11/2015 3:16 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello Parthiban; I would like to point out that normally Siemens processors use Industrial Ethernet for their Ethernet communications, not raw TCP/IP (unless they are specifically programmed to do so). There are many gateways that convert the 2 protocols, here is one standalone product I have worked with in the past: Prosoft is an Encompass partner of Rockwell Automation, and they also produce In-Chassis modules for the different Rockwell platforms, i.e. communication modules that plug directly in the racks of a Controllogix, Compactlogix or other CPUs. They are even easier to program than a standalone gateway, being designed for a specific Rockwell platform. Here is a converter module (Ethernet IP to Siemens Industrial Ethernet) for a Controllogix processor. You can find other platform converters depending on what you are working with, if you open the "!Rockwell Automation In-Chassis" tab: Contact a Prosoft distributor directly (there is a "Where to Buy" tab on the Prosoft Technology page) to find out pricing and availability of these products near you. One more option I have used in past projects, not exclusively for Ethernet IP conversion: the DSP gateway from Red Lion Controls. This is a generic protocol converter, with over 300 protocols integrated in the software (which is a free download), and can convert serial and Ethernet protocols from any number of automation providers. Have a look at their flyer for the DSP: MODEL DSP – DATA STATION PLUS - Red Lion Controls
Look at www.redlion.net for information on pricing and distribution. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 11/11/2015 3:32:30 PM |
|
Follow us on