4/24/2020 7:58 AM | |
Joined: 11/30/2016 Last visit: 9/3/2024 Posts: 19 Rating: (1) |
Hello I need to change the value of Numerator, Denominator and LeadScrew in the PositioningAxis technology object to change the gear ratio. I tried to do this during program execution, but I get a write access error in the PositioningAxis block. Being able to change values while the program was running made my life a lot easier. The ability to change the values of Numerator, Denominator and LeadScrew is logically necessary for axles with variable gear ratios during operation. Why Siemens decided to make them static is incomprehensible to me. Can I expect in future versions of MotionControl to implement this feature if not through direct editing (PositioningAxis.LoadGear.Numerator), then through additional MC_functions. Method suggested here it does not suit me. Regular rewriting of the MС-card will lead to damage. Although the method should be working, it complicates programming.
|