8/13/2018 12:35 PM | |
Posts: 8 Rating: (0) |
Hello Experts, I am working on IOT 2020 module in which when i start with "Hello World" Example which is given by default to connect with IOT 2020 Gateway module. When i am going to connect it to eclipse neon as per given step by step guide. i am getting error and not connecting to the IOT 2020 Module. Here i am attaching the error image file. And i build project two-three time but i am not getting any binary file in the project. Pinging to my module is also successful but not connecting with eclipse neon. Please support me. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/13/2018 2:01:36 PMNew subject after splitting |
|
8/18/2018 6:28 AM | |
Posts: 8 Rating: (0) |
Hello, Find attached image in which i had mention Putty connection Configuration and my network connection detail. I have connected IOT 2020 with my CPU which has two connection of network as per image file. both are working on seprate IP adrress. IOT2020 is connected through TPlink Ethernet to USB converter. AttachmentSiemens Error.docx (215 Downloads) |
Last edited by: Mr. Bhavsar at: 8/18/2018 6:29:19 AM |
|
8/20/2018 10:40 AM | |
Joined: 2/20/2014 Last visit: 9/17/2024 Posts: 396 Rating: (38) |
Hi Mr. Bhavsar, Can you let us know if you are trying to hook up the IOT now (first step to test if what the reference document showing is true). If you are just testing as per document. You can look for Node-red to understand & test out the IOT2020.. Besides, if you plan to grab some values from PLC into the IOT Node-red can still be used. If it is not a compulsory requirement to use Eclipse the trying looking for samples or steps on how to use IOT with Node-Red. This might let you move forward fast compared to waiting for solution on how to with Eclipse. |
8/21/2018 1:17 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello,
You can use Wireshark to find out the IP address of your IOT. In Wireshark, simply select your TPLink converter and klick on the shark fin. Kind regards! |
Follow us on