10/9/2018 10:43 AM | |
Posts: 7 Rating: (0) |
Hello People, I am trying to convert protool hmi file of SİEMENS simatic TD17 model to Wincc 2008 advanced sp2 but ı got error message which is ' No conversion available for this device' and it finish migration process. Could you please immigrate project that i have attached. Thanks ------------------------------------------------------------------------------------------ Attachmentrtg01td17program.zip (200 Downloads) |
Last edited by: The Helping Hand at: 10/9/2018 10:53:14 AMNew subject after splitting |
|
10/9/2018 5:23 PM | |
Joined: 9/21/2012 Last visit: 9/22/2024 Posts: 4157 Rating: (464) |
That means TD17 panel is not supported in WinCC 2008 SP2. The panel type has to be changed before migration. |
10/9/2018 6:30 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, there is no successor/migration for TD17 you can program only with PROTOOL please also look at page 16: |
Last edited by: Ste39 at: 10/9/2018 6:32:41 PM |
|
10/10/2018 2:01 PM | |
Posts: 7 Rating: (0) |
Is there any manual or instruction to do that? |
10/10/2018 3:38 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
No, there is a manual for TD17 (below): and for KTP 600 (below):
but pay attention KTP600 is in Phase Out |
Last edited by: Ste39 at: 10/10/2018 3:40:17 PM |
|
This contribution was helpful to1 thankful Users |
10/11/2018 7:35 AM | |
Posts: 7 Rating: (0) |
Thank you for your help. Also, ı immigrated the files of OP7 display to TİA portal version 11. I downloaded it to KTP600 via Siemens usb MPI adaptor but when i connect to the crane nothings seen on the display. I didnt change the simatic software, can it be the reason of that. Could you give some advice for this process. |
10/11/2018 11:45 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, did you check if all level in the template page is selected? |
Last edited by: Ste39 at: 10/11/2018 11:45:32 AM |
|
10/15/2018 9:51 AM | |
Posts: 7 Rating: (0) |
Do you mean Templates under the screen management section? 'Show all ES layers' is checked. And ı would like to know that do i need to change as well as simatic manager PLC Software of S7 300. Because protool hmı program is integrated in it. |
Follow us on