7/28/2011 6:31 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi, The diagnostic address of a SIMOCODE could not be directly read in the Device Configuration of STEP7 V11. This address is necessary to, for example, run a diagnose function of the module (DPNM_DG). To get this address, you can place the block (DPNM_DG) and select the SIMOCODE as symbolic name. This show a “basis” address. Adding 2, you can get the diagnose address of the module.The follow cast show how it is done. Attachmentdiag.zip (196 Downloads) |
Last edited by: Pegaia at: 7/29/2011 12:31 PMDenilson Pegaia |
|
This contribution was helpful to1 thankful Users |
8/1/2013 10:38 AM | |
Joined: 12/19/2011 Last visit: 10/13/2023 Posts: 1 Rating: (0) |
Mr Pegaia: It is posible to use the SFB51 or SFB52 for simocode. For S7-1200 |
Follow us on