1/19/2006 1:41 PM | |
Joined: 8/31/2005 Last visit: 10/23/2023 Posts: 217 Rating: (40) |
Hello Farzad! Check out this FAQ: "Chronological messaging in STEP 7 V5.2 and higher" It says "Chronological messaging means that the messages are sent from the PLC to the WinCC station. These messages then have a time stamp from the PLC." |
Greetings, Chris |
|
This contribution was helpful to1 thankful Users |
1/19/2006 3:10 PM | |
Posts: 43 Rating: (7) |
Dear Chris,
your advice is applicable only for S7-400CPUs but I have a S7-315-2DP.is there any other way? |
1/19/2006 6:21 PM | |
Joined: 8/31/2005 Last visit: 10/23/2023 Posts: 217 Rating: (40) |
No problem! [8)] Check out this link: Chronological signaling with S7-300 CPUs, STEP 7 V5.0 and WinCC V5.0 |
Greetings, Chris |
|
1/21/2006 6:38 AM | |
Posts: 43 Rating: (7) |
Hello Chris, |
Follow us on