12/20/2008 5:55 PM | |
Joined: 12/5/2006 Last visit: 5/26/2023 Posts: 177 Rating: (2) |
Dear UMENCHO Thank you But there is no problem in Disk Space. |
11/19/2013 3:26 PM | |
Joined: 11/19/2013 Last visit: 11/14/2022 Posts: 2 Rating: (0) |
Hi, I have exact the same problem. Does someone know what to do ? |
12/2/2013 10:51 PM | |
Posts: 38 Rating: (0) |
Its a disc space issue. I would double check where its beingsaved. "Message: Available space is less than the estimated image file size" |
12/3/2013 8:26 AM | |
Posts: 38 Rating: (0) |
Good morning, The Ghost image that you are loading, belongs to the machine, I mean if it is a previous ghost of the machine. |
12/31/2013 7:28 AM | |
Posts: 1 Rating: (0) |
Hi You may need to scale your image to solve the problem, which means adjusting the image size without changing the ratio between image width & height.To achieve this, an image processing control may be necessary. |
1/10/2014 12:34 PM | |
Joined: 11/19/2013 Last visit: 11/14/2022 Posts: 2 Rating: (0) |
Isnt there an "easy" solution like changing some Ghost options or so ? |