5/8/2015 1:07 PM | |
Posts: 18 Rating: (0) |
My question is regarding the global script functionality of WinCC (version 7.0 SP3). I have created a VB Script that logs a number of runtime tags to a text file. I have tested the script on a mouse action of a button without any issue. My next step would be to automate the procedure every hour. Here are the steps that I have taken thus far: 1. Ensure Global Scripts are running on the Engineering Station (As I have a Server-Client Architecture), by cheking that: WinCCExplorer->Computer\Properties-> {Engineering Station}->Properties->Startup TAB->Global Script Runtime ticked. 2. Ensure custom developed script is loaded into project, by checking that: WinCCExplorer->Global Script->VBS Editor->Actions->vbsLogFileB1.bas is loaded. · Note I have added a Cyclic Timer Trigger to the above script to run every minute (only for testing it will be changed to hourly once working) When I activate the project and leave the application running I do not get the output file every minute as expected. That’s basically where I am stuck at the moment. What am I missing? Any help would be appreciated! Thanks in advance! Juan AttachmentvbsLogFileB1.zip (107 Downloads) |
Last edited by: U_6a2c9b21-e041-40cc-9ef7-ce86863f8a30 at: 5/8/2015 1:08:09 PM |
|
Follow us on