4/13/2011 2:42 AM | |
Posts: 2661 Rating: (279)
|
Does your custom block creates EventState (alarms)? See the following: How should I configure a message block (FB43) so that it can be linked with a group display? |
This contribution was helpful to1 thankful Users |
5/8/2011 7:21 AM | |
Posts: 88 Rating: (0) |
Hiiiii, How did u solve? pls suggest,,,, Regards, Manoranjan |
5/8/2011 9:37 AM | |
Posts: 2661 Rating: (279)
|
Check the bits in the EventState variable. See Fig 01 in the following FAQ: How can you have alarms displayed in the process picture with the smart object "Group Display" when the bit alarm procedure or analog alarm is being used as the alarm process? Also see the following FAQ: What can you do if no messages are displayed in the overview area of WinCC? Regards |
This contribution was helpful to2 thankful Users |
7/17/2013 8:11 AM | |
Posts: 2661 Rating: (279)
|
Have you tried the following? a)Complete OS compile b) Run SSM c) Regenerate header in Global C scripts. Regards |
7/17/2013 10:45 AM | |
Posts: 62 Rating: (4) |
Dear Friend, Please do the below steps: 1.Deslelect Calc The Group Display &Delta Save Then Save the Picture Manager 2.Again slelect Calc The Group Display &Delta Save Then Save the Picture Manager 3. run the os project editor With Create& update Group Display for more details Please find the attached file. Regards, Avinashkrishna Bh
AttachmentGroup_Display1.zip (385 Downloads) |
This contribution was helpful to4 thankful Users |
1/31/2024 11:22 AM | |
Joined: 11/24/2021 Last visit: 4/25/2024 Posts: 1 Rating: (0) |
Kindly Share the steps to solve the group display issue |
Follow us on