Industry Online Support
Technical Forum
3/31/2012 6:32 AM | |
Posts: 2 Rating: (0) |
Dear friends, I want GSD file of TP 277 6' 6AV643-0AA01-1AX0 for the configure in hardware. |
3/31/2012 7:50 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, Which GSD files are there for the Profibus DP operator panels? In order to find is you should have WinCC flexible Standard or Advanced. Best regards, Hristo Mihalev |
3/31/2012 8:36 AM | |
Posts: 2 Rating: (0) |
Hello.. Ineed Siem813F.gsd file for using HMI LITE... |
3/31/2012 8:47 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Yes, this is the gsd file. best regards, Hristo Mihalev AttachmentSiem813F.zip (528 Downloads) |
Follow us on