Industry Online Support
Technical Forum
11/24/2008 12:24 PM | |
Posts: 2 Rating: (0) |
Hi, I have this scenario: CPU315 as MASTERmust communicate with a SLAVES7-224XP. Somebody could help me? Thanks. |
11/24/2008 1:55 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hi I think this is combination of Communication between S7-300/S7- 400 and S7-200 via MPI + Which settings do you need to make to access a panel and an S7-200 controller via TeleService? regards |
11/25/2008 2:52 PM | |
Posts: 5822 Rating: (412)
|
Hello, I have to admit, I have no solutions off hand for GSM, but how about GPRS? Check this out: Wireless Data Communication based on GPRS between S7-300 stations and SINAUT Micro SC Server Micro Automation: Wireless Data Communication based on GPRS (MAS 21) I think it is worth a moment to think about. Best regards J_Bell |
11/27/2008 10:16 AM | |
Posts: 2 Rating: (0) |
The communication between the 300 and the 200 can be direct ?
How much the hardware? |
Follow us on