7/4/2015 12:57 PM | |
Joined: 4/14/2013 Last visit: 3/28/2024 Posts: 28 Rating: (1) |
Hi! These Hall effect sensors, has thousands of different models. What model you want to use? What is its output? I myself have used the inductive sensors and encoders. A lot depends of the rotational speed in each particular case(whether the pulse rate of the received controller). E: The inertia of the conveyor: allowed start-up time, allowed constant speed, braking time and allowed max slip. Usually it is necessary to measure only these three main parameters. Then, the simplest option: measuring transducer must be not a main drive shaft and it may be sufficient only one sensor. (Circuit M-Al-1.lsc) E2: Or; measured anyway the difference between the shafts speed. Just build a safe, Avoiding self-starting and etc. (Slip control-1.lsc) AttachmentSlip-control.zip (166 Downloads) |
Last edited by: erku at: 7/7/2015 3:43:08 PMLast edited by: erku at: 7/7/2015 9:20:18 PM |
|
Follow us on