7/10/2019 7:00 PM | |
Joined: 4/28/2015 Last visit: 4/18/2024 Posts: 320 Rating: (35) |
Hi Shafay, What control system is your system running, 810D 840D pl/sl etc? Luke ...sent from App |
7/13/2019 12:18 AM | |
Joined: 10/17/2007 Last visit: 4/19/2024 Posts: 3969 Rating: (340)
|
Yes, you are right , you have option which copy past the "Simulation" files only. But Why i did not mention this at beginning --As tell you the truth, i myself also not sure where is the all files related to "Simulation" -- For 840C--I think it quit easy as the It is use DR DOS, the files is simple, I find SIMULATION path and copy past to the problem HD, --I am very lucky --I fix it at the 1st try. But I also prepared the another 2 solutions--I prepare whole HD Ghost and I prepared all data back up. --maybe you don't know --840C HDD is inside MMC CPU, when you withdraw MMC CPU from the control rack--there are some data lost. 840D MMC (old naame for PCU 50) is easy to touch HDD, but all files are Windows file You can tyr by yourself to find out SIMULATION files.-- Also you need to plan the machine down time (may affect 2 machine) also have risk (even less) to broken the HDD-- so if you think SIMULATION IS NOT SO IMPORTANT just let as it is. That is why I suggest using Ghost BTW--I don't suggest Ghost PCU50. 3C the using to PCU 50 Some PCU 50.3 C already use SSD another small tip--if you can find out --before SIMULATION frozen the whole PCU50, to see if there some message to show you what 1 or 2 files crashed or missing --you just copy --paste those files. I have done one time use this way to fix custom's PG-740 (Siemens PLC programming device)--usin Win95 |
Last edited by: nulizhang at: 07/13/2019 00:22:29Last edited by: nulizhang at: 07/13/2019 00:23:33try to find 1 or 2 files crash? If you like my comments please |
|
This contribution was helpful to1 thankful Users |
Follow us on