Industry Online Support
Technical Forum
5/17/2010 10:56 AM | |
Posts: 100 Rating: (2) |
Hi to all. I am using s7 300 PLC - 6ES7-313-5BF03-0AB0 and 8 channel analog module 6ES7-331-1KF00-0AB0. The cpu analog input and analog input card dont have Hart Input specility. In the field Emerson level transmitter Hart signal goes to Emerson PLC.The level Transmitter 24V DC source from Emerson PLC panel. Now i need the Level transmitter value in Siemens PLC too. If i use HART analog input module means can i get the value from level Transmitter(The 24V DC source is different) If the above can means (level transmitter hart terminal connected to siemens hart module then) how i should give hart input to Emerson PLC. Is it possible to tab parallel wire from level Transmitter. Could anybody help me. Is there any siemens analog module available with combination Hart Input and Hart Output. I have attached the detailed diagram below.
AttachmentHart input.zip (206 Downloads) |
Follow us on