9/5/2016 1:32 PM | |
Posts: 3 Rating: (0) |
Hello everyone, I have been reading about the Migration from Protool to Wincc flexible, and so far I see it is imposible for me to do so. I have WinCC flexible 2008 SP3 ( and I saw no Migration option) in Windows XP, and 2 Panels (MP370 and TP270B) with Protool V6.0 (but I have no Protool Software). I read I Need WinCC SP2 and some People offering to do such conversion, since they have an WinCC SP2 backup. Who would be so Kind to do such a favour? I zipped the all TDOP Directory, just in case. AttachmentTDOP.zip (79 Downloads) |
9/6/2016 8:14 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735)
|
Hello alvantan11 I have migrated it for you . you can find it in the attachment. There were 2 Panels so there are 2 Flexible Projects. I just migrated without testing or lokking at them after migration. I hope this helps you. Bye Murof Attachmentflex.zip (90 Downloads) |
Last edited by: Murof at: 9/6/2016 8:15:57 AMIf this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
9/6/2016 8:16 AM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735)
|
The second one I hope it will help you. Bye Murof Attachmentflex2.zip (81 Downloads) |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
9/6/2016 10:07 AM | |
Posts: 3 Rating: (0) |
Thanks a lot! I will take a look later and inform here how it goes. Thanks again. |
This contribution was helpful to1 thankful Users |
Follow us on