6/23/2014 7:29 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, which Scout and which Windows OS do you use? Regards Christoph |
6/24/2014 1:14 AM | |
Posts: 5 Rating: (0) |
Hello, Win7 64bit HP Computer Probook 6560b Scout V4.3.1 |
6/24/2014 6:24 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hello, here the sample project. You can simple import the XML Data for the lib and the program if the script didn't work. The lib is stored in: InterbranchSolutions_AxisFunctionBlock\LMCBasic_V1_2_3\LMCBasic_SIMOTION_V1_2_3\LMCBasic_SIMOTION\XML\LMCBasic The Unit ist stored in: InterbranchSolutions_AxisFunctionBlock\LMCBasic_V1_2_3\LMCBasic_SIMOTION_V1_2_3\LMCBasic_SIMOTION\Units If you would use a external SIMOTION Script on Windows 64bit you must use the Script interpreter which are stored in C:\Windows\SysWow64 (csript;wscript). If you doubleclick only on the vbe or vbs file the the 64bit interpreter is started an doesn't work wit the 32bit Application Simotion Scout. Regards Christoph AttachmentH:\Transfer\LMC_Example.zip (134 Downloads) |
Follow us on