5/24/2012 5:04 PM |
|
Posts: 8946 Rating: (999) |
One more reason NOT to use TIA. |
5/29/2012 12:07 PM | |
Joined: 8/31/2010 Last visit: 9/20/2024 Posts: 1521 Rating: (227) |
Hello IBN-Service, In WinCC v11 if we need to do the simulation with Tag Simulator, then we need to choose it from the Menu (Menu command "Online> Simulation> Start|With tag simulator"), whereas in WinCC Flexible there is a icon for that also. That's the difference i feel. The options are same in both WinCC Flexible and WinCC v11. Only the interface has changed a little bit. More info - Simulating a project (WinCC v11) |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
Follow us on