5/23/2012 8:00 AM | |
Posts: 4 Rating: (0) |
I have got a CPU S7 1200 1214 DC/DC/DC but i haven't got panel HMI KTP 1000. How do you do simulation on HMI panel.Thanks |
5/23/2012 8:14 AM | |
Posts: 8946 Rating: (999) |
Just start Runtime on your configuration PC that is connected to PLC. |
5/23/2012 2:24 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Now I check and it seems you will not start runtime for HMI |
Best regards, |
|
5/23/2012 6:32 PM | |
Posts: 8946 Rating: (999) |
Funny. I never had this problem. |
5/24/2012 5:04 PM |
|
Posts: 8946 Rating: (999) |
One more reason NOT to use TIA. |
5/29/2012 12:07 PM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello IBN-Service, In WinCC v11 if we need to do the simulation with Tag Simulator, then we need to choose it from the Menu (Menu command "Online> Simulation> Start|With tag simulator"), whereas in WinCC Flexible there is a icon for that also. That's the difference i feel. The options are same in both WinCC Flexible and WinCC v11. Only the interface has changed a little bit. More info - Simulating a project (WinCC v11) |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
Follow us on