9/21/2014 8:58 PM | |
Posts: 14 Rating: (0) |
pls show me how to check system software? |
9/22/2014 7:33 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
System menu > Service display > Version. |
9/23/2014 9:31 AM | |
Posts: 14 Rating: (0) |
i try with winpcin but not succed: - i power on my sinumerik, every thing is ok, no error - press ctrl + alt + N - press setpassword and enter the pass evening and accept - press IO data - select startup data pc and read in on my pc i open winpcin, select rs232 parameter, choose binary format - select send file and choose the startup file - the machinh restart sevaral times and then it show the error log DG.DIR\MDDRV.DIR\DRV1.TEA OK @@_N_ADRV_DP_MD_DRV1 Error! Code: 0x180 and the transfer is stop - i try alot but they has a same error i upload my startup file and the error image Attachmentchina.zip (272 Downloads) |
9/23/2014 10:29 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, After replacement of new PCU, have you loaded the set up file before loading back up? Please read the attched sheet for more detail information. Attachment802D setting the technology.pdf (409 Downloads) |
9/24/2014 4:04 AM | |
Posts: 14 Rating: (0) |
I readed this manual, but i don't have this setup file, could you send me this file or give me the link of 802d toolbox. |
9/24/2014 5:34 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
This file is available in tool box CD. Please contact Siemens for the same. |
9/24/2014 6:35 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
When you are reloading the back up, needs to connect with drive, MCP, KEY BOARD, PP module. |
10/21/2014 5:35 AM | |
Posts: 14 Rating: (0) |
Dear Mr PISCEAN 2010! I try as you said: I connect everything to sinumrik then first i download file settup_T, it success, then i download my startup file, my pc send success, but on sinumerik has transmittion error (image P1) : _N_CYCLE383T_SPF; PATH =/_N_CST_DIR OK Error! Code: 0x58 And on alarm windown has some error (image p2): 026015 Axis z1 machine data mn_drive_telegram_type[1] invalid value 026015 Axis x1 machine data mn_drive_telegram_type p915[0] invalid value 026015 Axis z1 machine data mn_drive_telegram_type p915[0] invalid value So i check machine data and found that all parameter 13060 drive_telegram_type are 0 (image p3), then i set those to value 102 and 104 (image p4) save and reset sinumerik, and there are no error remain, then i try to run machine every thing ok, drive x, z and spindle run ok, there no error occur but the spindle speed feedback no speed and on sinumerik has message Wait spindle (image p5) I replace spindle encoder but not success, i online simodrive 611 using simocom U and i can see encoder data change on profibus diagnostic frame, so i think my encoder is ok. My machine have 1 double motor module for drive X and Z axis, and spindle encoder is 6fx2001-2eb02 , it connect to X472 I guest parameter 13060 are not correct, so please help me setting correct machine data parameter Attachmentimage.zip (198 Downloads) |
10/26/2014 8:47 AM | |
Posts: 14 Rating: (0) |
in my machine par13070 is set 0f, now i must set it to 8000h? i read in manual 8000h mean deactive consistent check of profibus telegrame. is this right?
|
Follow us on