6/27/2018 2:58 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi, have a look to the manual of the module: SIMATIC S7-300 S7-300 Module data there is also a chapter that describes the principles of analog value processing(chapter 4). the functions you need to "convert" are called SCALE and UNSCALE. you will find them in Basic Instructions->conversion operations. See the TIA-help of the block, how it works. regard, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
6/28/2018 9:06 AM | |
Posts: 8 Rating: (0) |
Hey hi? Which convert do i need? I am beginner sorry hehe. I want to write 20 and my AO module should be out 20mA. Just i want do that. What can i do? |
6/28/2018 9:26 AM | |
Posts: 2826 Rating: (684) |
Hey mopS04 - You are being led down the garden path. The topic starter is still on the same topic as what you helped him with at https://support.industry.siemens.com/tf/in/en/posts/193806/. He is using the classic Step7 V5.5 with an S7-300. He should Read The Fabulous Manual you suggested originally. Cheers. |
This contribution was helpful to1 thankful Users |
Follow us on