9/23/2010 6:02 PM | |
Joined: 8/30/2010 Last visit: 12/8/2023 Posts: 31 Rating: (1) |
Hello Aret, You have given solution to handle 64 bit value in S7300, Its a really impressive. If you could help me to handle 64 bit value in S7200. It will be greate help. My complete project is based on this solution. OR is it relly possible to solve this value? I am reading values from MAG 8000 device on MODBUS RTU protocol in S7200 and sending to WinCC Through GPRS. I couldnt read Totalizer values from device for given register address. Regards, Jeetendra Splitted from How to handle data ?. |
Last edited by: O_Moderator at: 9/24/2010 9:47 AMLast edited by: O_Moderator at: 9/24/2010 9:47 AMnew subject after splitting |
|
9/24/2010 9:48 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread Reading 64bit value in S7200 PLC. Best regards O_Moderator |