7/16/2013 6:49 PM | |
Posts: 98 Rating: (6) |
I forgot about price on Software XD But Comparing to S7 200, even there's more info. you know that are free libraries from users so the information are somtimes a little bit confusing. RS232 is important as Maddoc said: "The most important thing is a full RS232 port: i need to do something like:.." So ethernet is an option but is an aditional; even so, is a good option but the function blocks required an IP direction (is what I remember) so on different PC's there are some things to configure. William B.On Logo! is there any option RS232? I haven't managed it on communications process
|
7/16/2013 8:44 PM | |
Posts: 621 Rating: (9) |
Hello. you are devloping the your small maximum 10 DI/DO. so PLC S7-200 PLC 224CPU.and TP177mono.
|
7/17/2013 12:25 PM | |
Posts: 1064 Rating: (72) |
engineering station for programming (es) |
This contribution was helpful to1 thankful Users |
7/17/2013 2:44 PM | |
Posts: 98 Rating: (6) |
My mistake I wrote on spanish E/S means I/O than Inputs/Outputs Sorry |