Industry Online Support
Technical Forum
6/14/2012 4:13 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello, please follow the link to find some possible motors: https://intranet.automation.siemens.com/mcms/mc/en/motors/motion-control-motors/simotics-s-servomotors/Pages/synchronous-motor.aspx Relating high dynamic by less motor inertia the 1FT7 is a very good choice. E.g. 1FT7066-xAF with 2,92KW @ 3000upm Controlled could be the motors via SINAMICS S120. The point 4 will be a problem. Becausethe smallerSiemens motors (1FK/1FT)have no integrated clutch. Maybe you canconnectan external clutch. |
With best regards, |
|
6/14/2012 8:57 PM | |
Posts: 767 Rating: (69) |
Hello, I agree that the point # 4 is not available from Siemens motors in this size range for 1FT/1FK servo motors. Attached is a sample bill of material for motor and drive system. Note: The motor in bill of material does not have a holding brake. If a holding brake is needed then bill of material would need to be modified slightly. You can look at drawing for motor by viewing on website at CAD CREATOR tool. http://staging04.it-motive.de/CADCreator/VorNavigation.cfm?IdListVornavi=(0-1*906)&CFID=4412387&CFTOKEN=22532204&Scenario= Best Regards, Deputy Attachment1FT7066 Example.pdf (352 Downloads) |
Follow us on