12/7/2019 6:44 AM | |
Joined: 6/25/2015 Last visit: 3/18/2024 Posts: 3 Rating: (0) |
I have a LOGO application where I want to change a time parameter on an on delay timer via an HMI KTP700. The current set time is displayed on the HMI. My problem is how do I take the time value from the HMI and change the On Delay time on the LOGO? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/09/2019 11:05:19New subject after splitting |
|
12/7/2019 8:01 AM | |
Joined: 12/18/2014 Last visit: 4/20/2024 Posts: 32847 Rating: (4061)
|
Hello Ngonji, in attachment an example with a possible solution. TIA V13 SP2 and LSC V8.0. AttachmentKTP700 with LOGO!8 timer setting.zip (241 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on