Industry Online Support
Technical Forum
7/23/2014 12:37 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! Nothing special in your requirements, but i have few questions to ask: 1. If you plan to integrate new automation cell to existing plant, please specify configuration you already have. Depend on this we can suggest you right solution based on distributed stations, PLCs etc. 2. If you wish to build completely new, separate automation cell, based on specification you provide I can suggest you to look at S7-300 series PLC. It is very universal, mid-size modular PLC with al option you asked available.Hereis a good starting point for S7-300. Another links: 1.Simatic brochurewith differences of PLC families. Hope it helps. Feel free to ask additional questions. I'm sure you'll have) |
7/23/2014 1:00 PM | |
Posts: 4 Rating: (0) |
Thanks a lot for your quick response. I will have further enquiries for sure. |
7/23/2014 2:31 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! You do not need any special communication module for web-server functionality. However, web server of profinet device wil give you only limited amoun of infomation, such as preconfigured diagnostics, error messages, etc. For control and monitoring you can choose a Simatic panel or a PC with SCADA software. Depending on model they are able to communicate via ethernet of profibus. Also, choosing of HMI system depoends on task, on process, and your automation needs. For distributed IOs please refer tothis link. For high-voltage measurement and control Siemens haveadditional departments. These are separate from automation.To choose a solution you should provide more details on the task: e.g. it is substation automation, power qulity measurements, etc. |
7/23/2014 2:36 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Addition: For S7-300 module data refer to this link. You can find all available measuring ranges (data is given for 6ES7331-7KF02-0AB0) Voltage ± 80 mV ± 250 mV ± 500 mV ± 1,000 mV ± 2.5 V ± 5 V 1 V to 5 V ± 10 V Current 4 mA to 20 mA ± 3.2 mA ± 10 mA 0 mA to 20 mA 4 mA to 20 mA ± 20 mA Resistance/Temperature 150 Ω 300 Ω 600 Ω Pt 100 Klima Ni 100 Klima Pt 100 Standard Ni 100 Standard Thermocouple Type N [NiCrSi-NiSi] Type E [NiCr-CuNi] Type J [Fe-CuNi] Type K [NiCr-Ni] Type L [Fe-CuNi] |
7/23/2014 2:46 PM | |
Posts: 4 Rating: (0) |
Thsnks again. This is really helpful. |
This contribution was helpful to1 thankful Users |