Industry Online Support
Technical Forum
4/28/2011 10:03 AM | |
Posts: 2 Rating: (0) |
hi all I have six s5 115uplcs and two operator stations thatconnected together with profibus fmsthrough the fiber optic network (attached schematic).operator stations are using a very old hmi software (gepro6)so i want to replace gepro softwarewith wincc .for this i used a wincc v6 sp4 and simaticnet 2006 software on windows XP sp3andcp 5613a2 in pc side for connecting wincc station tothe fms network. In the existing system (old system)a cp 5412a2 isused in thepc side(operator station)and cp5431in plc side. i configured pc station and wincc as siemens documentand at first i try to make a connection between wincc and one of thesix plcs,butwincc can't connect to the plc. It seems that cp 5613 work well and communicates in the network but wincc can't connect to the plc and in wincc channel diagnostic, i have "no connection to wincc "message. Thank to any bodyhelp me in this problem sorry for my bad english speaking I attach configuration sheets for cp5431 and wincc and also project file of pc station to this post. Attachmentnetwork schematic&configuration.zip (64 Downloads) |
Last edited by: tolid at: 5/1/2011 12:07 PM |
|
4/28/2011 11:15 AM | |
Posts: 799 Rating: (42)
|
Dear tolid, I never worked with S5, because I'm to young for this, but there is an faq, which can be very useful for you I think. S5 FMS link to WinCC Hope this helps you |
Follow us on