3/12/2020 6:07 AM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
Hello freiz, I don't understand this part of your question
For what reason do you want to use the flags to switch the outputs? You can use the cursor keys of the LOGO! (or of the TDE) and the F-keys of the TDE can be easily integrated into the program like normal buttons on digital inputs. When using the cursor keys you only have to note: You can also include one or more softkeys in a message text and use it to switch on the display. AttachmentKeys_0BA8.Standard.zip (173 Downloads) |
3/12/2020 12:37 PM | |
Posts: 25 Rating: (0) |
Hello, thanks for your help. Sorry my English, I don't have much experience.
AttachmentC logo Keys.zip (168 Downloads) |
Last edited by: freiz at: 03/12/2020 13:24:34 |
|
3/12/2020 2:04 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
Depend on your concept you also can multiply the function of the F-Keys. There are several ways to do this: 1. Use a hardware or software switch to differ between normal mode and service mode, then you can use F1, F2, F3, F4 for different functions, see example in attachment 2. Use a counter with F1=Up and F2=Down and select your messages separate depend on the different counter values. Then you can use the F3 and F4 key for different functions in every message. If you have only few messages, you only need 1 key to cycle your messages and have 3 keys for different functions There are more ways possible, but i don't want to write a novel. Regard, Scorp AttachmentService-keys.zip (185 Downloads) |
3/12/2020 3:39 PM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
I tested the program in my LOGO! and it works coorect. The second softkey as switch turned Q2 on/off. |
Follow us on