3/3/2015 1:51 PM | |
Posts: 5 Rating: (0) |
Hi, The hmi connection I have configured does not work. I have an error message which I got after the update to SP1 (Wincc Prof v13) "The PC interface is not assigned to the simatic pc station. Please assign the simatic pc station to the local interface in the interface assignment in the inspecotor window" As simple as is sounds. I have no idea what I need to do. I have attached there one image with three partial screen shots. The first displays the error message. The other two display my current settings. At the third screen I can choose for PC Station V1.0. But it think I dont have S7-RTM installed. If I choose PC station, in the second screen PC Station comes available. After that it hangs on the hardware download. Do I need to install some sort of PC Station software, on the Client or ES. There is an other topic about the problem. But I now know it has noting to do with the visualisation. So I decide to repost it here. This time with the problem in more detail. Kind regards, SRobijn |
3/11/2015 9:16 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
Closed cause question posted twice.
|
Follow us on