1/9/2019 8:01 PM | |
Posts: 4 Rating: (0) |
I'm owning a CarPlay head unit from Volkswagen called RCD330 plus. It is possible to upgrade/downgrade to any available firmwares. The firmware file itself is a *.tar file and can be extracted. I found a linux file structure (var, etc, opt, ... folders). My goal: The head unit supports only a few languages like Chinese, Mexican, US English, ... and I want to add support for German language. What I tried already (1) I checked nearly every file with a HEX editor (iHex for Mac OS X) and found one 9.4MB big file called hmi(without extension) in folder/opt/and this file contains all labels:Screenshot_18.jpg you can see hmi file here : [snip] Where can I get information/knowledge to add an additional language. Maybe also with adding german language flag in the setup menu of the radio? Or is this just impossible? Is thishmifile a compiled file or is it kind of some archiv which can be somehow extracted? Attachmentfiles.zip (114 Downloads) |
Last edited by: fatihfx at: 1/9/2019 8:02:49 PMLast edited by: fatihfx at: 1/9/2019 8:03:32 PMLast edited by: Jen_Moderator at: 1/10/2019 7:40:41 AMRemoved link and added file as an attachment. |
|
1/10/2019 6:57 PM | |
Posts: 4 Rating: (0) |
I dont know, I hope. |
1/10/2019 6:57 PM | |
Joined: 12/18/2014 Last visit: 9/21/2024 Posts: 33809 Rating: (4200) |
That's not WinCC. |
1/10/2019 7:00 PM | |
Posts: 4 Rating: (0) |
can you check hmi file ? look the attachment. Attachmenthmi.zip (98 Downloads) |
Follow us on