2/26/2019 3:33 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641) |
Hello HIM61 ??youhave a Panel that has no Ethernet Port???? so what do you want to do? in your picture we can see a DP Connection, no Ethernet Connection. and your Panel can only run DP/MPI So use a Panel or a PC Based Runtime that can be used with Ethernet and then: https://support.industry.siemens.com/cs/ww/en/view/24109937 Bye Murof |
Last edited by: Murof at: 2/26/2019 3:36:06 PMIf this Information really helps, you could use the Rate function |
|
3/7/2019 4:14 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641) |
Hello OK now i Understand what you are talking about -> If you want to transfer the HMI Project then check this out: https://support.industry.siemens.com/cs/ww/en/view/32235096 -> But If you want to Start your Runtime or Simulation on Engineering PC then you cannot communicate with the PLC its because you have a MPI/DP Connection in your HMI Project and not an ethernet Connection. You also can use a routing Connection but then you will have to change you complete HMI Project and the Connections. so I would not do that. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on