Industry Online Support
Technical Forum
10/8/2014 2:51 PM | |
Posts: 1299 Rating: (135)
|
Hello, seems like you have no connection to the plc. do you simulate the plc with s7-1500 plcsim like mentioned in the other thread? K!ke |
10/8/2014 7:54 PM | |
Posts: 124 Rating: (4) |
my connection to plc is virtual, I want to control PLC by HMI in simulation. I attached my work, when i push "motor (out)" button in HMI, the output changed but when i push "start" button also in HMI, no event occurred !!!! I think only output works, and for input i must buy PLC! Attachmentmy work.zip (237 Downloads) |
10/9/2014 12:50 PM | |
Posts: 124 Rating: (4) |
Thank everybody. I should use plcsim and simtable to change input value. |