1/15/2020 10:57 AM | |
Posts: 2 Rating: (0) |
Hey, thanks for the quick reply. I think I've not explained the situation very well. What I'd like is for the data to be processed in program, so that a warning can be raised as soon as an issue arises. We're adding this in due to having several pumps failing due to them running dry with the system we have installed currently. I've got a copy here of what I've managed to get done so far. I've also run into an issue of not being able to connect a contact to reset a pair of counters... I'll try and figure that out on my own though. AttachmentLW leachate lvl monitor prog.zip (144 Downloads) |
1/15/2020 11:16 AM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33813 Rating: (4201)
|
Which contact should reset the counters? |
1/15/2020 12:56 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Maybe you only need some information, how to store an analog value. For this use mathematic operation with parameter checked "last value" or the min/max block, see example in attachment. Regards, Scorp AttachmentAnalog storage1.zip (199 Downloads) |
Follow us on