1/1/2014 4:08 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello basebalaji; If you plan on working with Siemens automationequipment, the only configuration that will support "Hot Redundancy" is a Fault-Tolerant S7-400H system, that you will find described in this manual: SIMATIC Fault-tolerant systems S7-400H S7-400H: Two CPUs specially designed with a high-speedfiber-optic linkand set up as active/standby pair to continuously update bothcontrollerson process values make up the hot-redundant system. Switchover time is calculated in ms, and it is triggered by the detection of critical faults.by the CPU's OS. A possible option is "Software Redundancy", which allows a pair of CPUs in the S7-300 and S7-400 to use standard communication networks to switch when a fault is detected in the active CPU. In this case, this is considered a "Warm Standby" system, switchover cantake up to a few seconds depending on the network selected for redundant functions, and all the programming for the redundancy functions must be done by the programmer. See the following information: SIMATIC S7-300/S7-400 Software redundancy for SIMATIC S7 As you can see, there is noeasy and simple reply to your original question. The S7-200 and S7-1200 families do not suppoort redundancy (Note:it is possible that the S7-1500 CPUsoffer it in the forseable future), so your options are limited to the above packages. Study the information provided, and come back to the forum if you still have questions. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/1/2014 6:39 PM |
|
This contribution was helpful to2 thankful Users |
1/22/2014 1:53 PM | |
Joined: 8/20/2011 Last visit: 9/17/2024 Posts: 22 Rating: (0) |
see the below links
|
Follow us on