3/25/2021 9:29 AM | |
Joined: 9/24/2013 Last visit: 9/19/2024 Posts: 36 Rating: (0) |
Hello. I want to make a "HOT Swap" of the memory card in the S7 1512SP F-1 PN. I don't have the siemens MMC reader, but a have the same CPU on my desk with 24MB MMC. The F-safe faetures are turned off in the CPU. I'd like to know if i will follow the procedure: 1. Upload the project from working CPU. The process will keep runnig from the point when the power supply was turned off ? Edit: As the situation was urgent, i have tested on other CPU's . The procedure worked perfecty. After the return of power supply the system continued the process with the stored in the memory retentive data of actual state. ------------------------------------------------------------------------------------------ |
Last edited by: Sliwka at: 03/25/2021 11:04:29Last edited by: Jen_Moderator at: 03/25/2021 11:42:56New subject after splitting |
|
This contribution was helpful to1 thankful Users |
Follow us on