7/26/2014 8:12 PM | |
Joined: 8/2/2011 Last visit: 10/9/2022 Posts: 12 Rating: (0) |
Hello, I'm trying to make HOURS COUNTER on LOGO 0BA7 and that time show on HMI panel (KTP400) but I have problem with representation of results. On LOGO value is 5:00 and on HMI is 300. I tried to change "Display format" in WINCC, but no results. Do anyone know how to set TAG, DISPLAY FORMAT on WINCC so the value on LOGO and HMI will be same. In Attachment are photos of settings. Thank you. AttachmentLOGO+HMI HOURS COUNTER.zip (499 Downloads) |
7/27/2014 11:12 AM | |
Posts: 5225 Rating: (1185) |
Hi there, [personal notes / opinion] I am disappointed to learn that you have given up on the display of the hour counter. Surely there must be a good reason why you were thinking to put it on the HMI. Surely showing it in minutes would not be THAT bad. Personally I would re-engineer the hour counter to have two parameters. It is good that you are asking all these questions. Keep in mind however that the LOGO is marketed as a "Programmable relay". If Siemens put too many functions in the LOGO it will reduce the S7-1200's business. Get whatever you can get from the LOGO, but expect limitations.. so do your homework well. If you have not done so already.. get the System Manual for the LOGO. [adjusting time and date from HMI] I am of the opinion that you will not be able to edit the time/date of the LOGO with a "normal" HMI. I would expect the LOGO-TD (external text display) should be able to do more. Synchronising will not be possible (my opinion). Maybe the experts have more on this.
[special flags] Are sure you wish to know about M24?.. Are you sure you are not thinking of M8?
Please look at the thread.. [LINK] Other special flags exists.. I would encourage you to read the HELP given by the software or have a look at the System Manual. I hope this cover what you asked about. Greetings for now. w |
10/29/2014 3:41 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on