2/13/2022 8:59 AM | |
Joined: 2/24/2015 Last visit: 10/11/2023 Posts: 2 Rating: (0) |
Hello dear friends. In the system of s7400 plugin and server, how can I check the connection between server and plc in software, while the connection between plc and server system is established via mac address. Thank you for your help. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/14/2022 11:51:26New subject after splitting |
|
2/16/2022 9:28 AM | |
Joined: 8/3/2009 Last visit: 5/13/2024 Posts: 12933 Rating: (1646) |
Hello hamedzahedi which WinCC Version do you use? Are you communicating with Industrial Ethernet in Simatic S7 Protocol Suite? Check out this FAQ: https://support.industry.siemens.com/cs/ww/en/view/382120 Or do you want to know in PLC if the WInCC is offline? then you can do a Handshake with Timer in the PLC and WinCC and then if the timeout runs out and WinCC is not answering then you know it in PLC. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on