7/30/2020 1:41 PM | |
Joined: 9/20/2017 Last visit: 3/20/2024 Posts: 27 Rating: (0) |
I am using simatic wincc (TIA Portal v15) to monitor the data to be received from total 54# slave devices via Modbus RTU Protocol. I have used total 4# gateway module (i.e. Schneider EGX300) to convert the data from Modbus RTU to TCP/IP. All 54# slaves are transmitting data via Modbus RTU in daisy chain on all 4 gateway module. My problem is that, i need to create total 54# connections if i consider the 1 connection for each slave. and TIA Portal is allow maximum 8 or 16 connection. now problem is how can i communicate all that devices together with my wincc software. ------------------------------------------------------------------------------------------ |
Last edited by: paresh_ramdya at: 07/30/2020 13:47:02Last edited by: Jen_Moderator at: 07/31/2020 08:06:25New subject after splitting |
|
Follow us on