12/24/2017 8:26 AM | |
Posts: 11 Rating: (0) |
I have siemens S7200 PLC Model No:CPU 224 XP CN Expansion Module Model No:EM223 CN Model No:EM222 CN Model No:EM232 AQ4 PC config:windows 8.1/micro win v4.0 while I am connecting with CPU I got the communication between PC & PLC . but I cant able to download . I cant able to configure EM expansion modules. Its showing un fatal error. here I attached the snap of the program for Downloading & EM configuration kindly suggest the exact procedure. AttachmentPGM_SNAP-EM config.docx (243 Downloads) |
Last edited by: Rajendiran A at: 12/24/2017 8:27:18 AM |
|
12/24/2017 8:38 AM | |
Posts: 11 Rating: (0) |
I have siemens S7200 PLC Model No:CPU 224 XP CN Expansion Module Model No:EM223 CN Model No:EM222 CN Model No:EM232 AQ4 PC config:windows 8.1/micro win v4.0
its showing un fata error kindly suggest the exact procedure.
AttachmentPGM_SNAP.docx (187 Downloads) |
12/24/2017 11:32 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, I can recommend S7-200 System manual: S7-200 System manual |
With best regards... |
|
12/24/2017 12:22 PM | |
Posts: 11 Rating: (0) |
kindly refer the link for S7 200 manual |
12/28/2017 6:04 AM | |
Posts: 11 Rating: (0) |
I checked the possibilities to download the program in cpu 224 CN I didn't get it kindly suggest the procedure for factory resetting CPU 224 CN Regards Arul |
6/27/2018 2:39 PM | |
Posts: 6 Rating: (0) |
Hi, Thank You advice!!! |
Follow us on