11/18/2014 10:08 PM | |
Posts: 2 Rating: (0) |
How can I Configure SM1231 for 1-6V AI 8x13Bit 6ES7 231-4HF32-0XB0 TIA V13 Properties List: Analog input module AI8 x 13 bits; plug-in terminal blocks; input: 2.5V, 5V, 10V and 0 to 20mA; configurable frequency suppression; configurable smoothing; configurable diagnostics On Power up: All red lights flashing on SM1231 module Have 25.7V power to L & M Go online: 1 problem found. How do I tell what problem was found? Thanks
|
Last edited by: Min_Moderator at: 11/19/2014 8:48 AMSplitted Last edited by: Ken7322 at: 11/18/2014 10:36 PM |
|
11/19/2014 3:07 PM | |
Joined: 7/7/2010 Last visit: 4/18/2024 Posts: 14594 Rating: (2347)
|
Without additional hardware, configure for +/-10V and scale to meet your needs. Have you downloaded the plc hardware configuration? Have you grounded ununsed AI's? |
science guy |
|
7/19/2015 12:51 PM | |
Joined: 10/31/2013 Last visit: 4/17/2024 Posts: 6 Rating: (1) |
What will happens if there is no input connections......? I'm getting a problem, my AI values are fluctuate in a large range... How can I solve this...? Plzz Help Anyone.... Arafat |