10/9/2009 9:44 AM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168) |
Dear drozerce, It will take some time to read in log. Have you seen this link: how are tags and alarms logged in WinCC flexible? Best regards, Wizard |
10/9/2009 9:54 AM | |
Joined: 4/24/2006 Last visit: 9/18/2024 Posts: 8738 Rating: (1168) |
Dear drozerce, Have you seen this link: what options are there for creating a screenshot in WinCC flexible ES, Wincc flexible Runtime or on panels? Best regards, Wizard |
10/11/2009 8:36 PM | |
Joined: 6/3/2009 Last visit: 9/14/2022 Posts: 118 Rating: (2) |
Dear all, Thanks for the manuals but they didn't help very much. First of all the manual How tags and alarm archiving in Wicc Flex chater 2.4 says that is for Wincc Flex version 2008. I'm using version 2007. Another thing is that I configured the trends but I couldn't understand from the manual how to increase the Log time, for a day. I saw how to configure them, but not to increase the time of loging trends. Another strange thing happens, every time when I open the trend window, every time I can see log trends for a different time back. First time only two hours, second time half hour etc. Also I coppied the file, where trends are loging, from OP panel to my PC using USB. And when I opened there was nothing in it (see attachment 1). I think that they are suppose to be fulfilled with something, isn't so? To get back to increasing time for trends, in addition I'm sending you3 attachments. First one is how my trends (tags)are configured, the second one is how Data log is configured and the third one how is trend window configured. So if I'm doing something wrong please tell me.Thanks AttachmentTrends Problem.zip (184 Downloads) |
10/13/2009 4:28 PM | |
Joined: 6/3/2009 Last visit: 9/14/2022 Posts: 118 Rating: (2) |
Hellooo anyone help!!! Does anyone knows something? Please!!! Thanks |
Follow us on