12/23/2018 1:55 PM | |
Posts: 4 Rating: (0) |
Hi, i tried to run a 3g connection with a PCIE Huawei module with ppp and wvdial. When all is right configurated I will start an connection test I bekome an error. > The PPP daemon has died: Pty program error (exit code = 9) messages log: Dec 8 16:04:06 localhost pppd[2866]: pppd 2.4.5 started by root, uid 0 Dec 8 16:04:06 localhost pppd[2866]: Using interface ppp0 Dec 8 16:04:06 localhost pppd[2866]: Connect: ppp0 <--> /dev/ttyACM0 Dec 8 16:04:06 localhost pppd[2866]: CHAP authentication succeeded: Congratulations! Dec 8 16:04:06 localhost pppd[2866]: CHAP authentication succeeded Dec 8 16:04:06 localhost pppd[2866]: kernel does not support PPP filtering Dec 8 16:04:36 localhost pppd[2866]: IPCP: timeout sending Config-Requests Dec 8 16:04:36 localhost pppd[2866]: Connection terminated. Dec 8 16:04:36 localhost pppd[2866]: Exit. Dec 8 16:04:06 localhost pppd[2866]: kernel does not support PPP filtering I think this will be the problem. How can i install/aktivate the PPP filtering support? Thanks. Tim ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/6/2019 11:31:34 AMNew subject after splitting |
|
1/7/2019 1:19 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, We have an application example for the usage of 3G cards if you are using the example image provided by Siemens. If you are using the Debian image on the other hand, we cannot give any support for it on this forum as it is not an official image. It appears the ppp filtering module was not included in the kernel config during compilation. To fix this, I suppose you will either need a rebuilt image or a kernel patch. Kind regards! |
Follow us on